Other Parts Discussed in Thread: TLV320AIC3101
Hi Team,
A customer is looking into using them in an intercom-like application where there would be one microphone broadcasting to 4 speakers. This would require relatively low latency, but high enough to be easily obtained by this module. The concern is for this application there will be many of the same types of networks in close proximity that could cause interference.
In the user guide, it recommends no more than 4 networks should coexist, but this testing was done with the network's broadcasting 40 cm apart, for the application they would be 30-40 feet apart. By reducing the audio sample rate, having only 1 audio channel, disabling audio fade-out, sending audio only from master to slave, and not increasing output power too much would it be enough to not have excessive interference?
In addition, If they would like to use it autonomously, but need to include an IC for a battery fuel gauge indicator, can the cc8530 be master in i2c communication or can the cc8530 only be a master of external audio IC? Also when using the device autonomously in an end product, is there a way to communicate with the IC once in the embedded system for troubleshooting, firmware updates, or part service, i.e. uart port, USB port, or wireless interface?
Thanks in advance.
Regards,
Marvin