This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RF430FRL15xH
What is the optimum or target coil inductance to add to a RF430 (TI RF430FRL15xH) to achieve maximum performance / range?
The on-chip resonance capacitor (CINT) has a typical value of 35 pF, which without any additional parallel tuning capacitor would require an antenna coil with an inductance of circa 3.9uH.
But I could arbitrarily design a range of coils (and inductance) to resonate with the RF430 by adding the necessary external resonance capacitor parallel to CINT. A CINT of zero would require 3.9uH (the maximum inductance), but the minimum has no theoretical limit, e.g. 50pF with a 2.7uH, 100pF with a 1.4uH, 1nF with a 137pH, 2nF with a 680pH and so on.
I thought increasing the coupling of the reader antenna to the tag antenna should increase performance and, simplistically, increasing the turns on the tag antenna should increase coupling (assuming the same tag area), so as I reduce the tag coil inductance and reduce the number of turns, but increase the external resonance capacitor to compensate, I will reduce the coupling.
But there must be an optimum, or a target value which optimises performance, but I cannot find any recommendation in any RF430 application note. SLOA217A states "5.2 External Antenna Inductance Range Without External Capacitor, Theoretically, the antenna inductance can have any value within the logical range of the L/C ratio", which implies simplistically, (a) choose a coil design, (b) measure its inductance, then (c) tune.
For the TRF79xx reader, SLOA241C (Antenna Design Guide for the TRF79xxA) states "....it is ideal to target for a coil inductance in the range of 1 to 1.5 μH” (but it doesn’t say why).
The RFID Handbook from Klaus Finkenzeller, page 75, suggests that there is an optimum tag antenna (circa 1uH).
Do you have a recommendations, my project requires maximum range with minimum tag size.
Hello Customer, thank you for your question and interest in our products.
The forum support of this product has been reduced to first reference our existing documentation and collateral. For support, please take a look to the “Similar Topics” section at the lower right of the thread page. In addition, please consult the existing collateral in the “Technical Documentation” section of the RF430FRL152H product web page along with the Frequently Asked Question document. Alternatively, you can use the search engine of your choice to look for related E2E threads. With each of these resources we believe it will help with your question.
sloa247c "Frequently asked questions for RF430FRL15xH devices" refers the reader to sloa217a "RF430FRL15xH NFC ISO 15693 sensor transponder practical antenna design"
217 states a value for the onboard antenna of 1.8uH, but states "Theoretically, the antenna inductance can have any value within the logical range of the L/C ratio." and provides a graph showing L-C combinations
The example Application Circuit in the datasheet slas834c shows a 3uH inductance.
If I wanted to design a 25 mmx 35mm pcb antenna, then (these figures are approximate to illustrate the point), I could wind: 4 turns for 1uH, 5 turns for1.5uHm 6 turns for 2.0uH and so on.
Surely, there must be an optimum. I always thought more turns captured more flux, which should lead to more harvested power?
Is there another document that I should read?