1 Watt RF3858 PA and CC1101
AN101 "Using 1 W RF3858 Front End with CC1101 under FCC 15.247" outlines the expected performance when using a RF3858-CC1101 design under FCC Section 15.247 in the 902-928 MHz frequency band. The RF3858 is a single-chip front-end module from RFMD. The maximum output power for the combined solution is 1 W and the sensitivity is improved 5-6 dB compared to a CC1101 stand-alone solution.
App note is available from http://www.ti.com/lit/swra377 and reference desing from http://www.ti.com/lit/zip/swrr085