Hello Everybody,
I wan to use the CC2420 with the MSP430F1222 MCU and here is my question:
What pins (minimum!!!) do I need to transmit and receive data from/to the CC2420. Is it enough to interface the CC2420 with the three SPI Pins (SI/SO/SCLK) ?
What happens to the other pins (FIFO,FIFOP,CCA,CSN...etc) that I see in a all of the example applications in the datasheet?
Another question:
I don't want to use the internal voltage regulator of the CC2420. What should I do with the VREG_EN, VREG_IN, VREG_OUT pins. should I leave them unconnected.
Thanks a lot!
Mario