This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2570 32K Hz crystal optional?

Other Parts Discussed in Thread: CC2570

Hi,

I am looking at the CC2570 vs the Nordic AP2. The Nordic chip can synthesize the 32K Hz clock from the external 16 MHz clock, is this possible with the CC2570 or is the 32k Hz crystal required. If it is possible to use the CC2570 without the 32k Hz crystal do the input pins for the clock (XOSC32K_Q1, Q2) need to be tied to Vcc or Gnd?

Also, I see that the reference circuit documentation (SWRC225.zip) uses a 32 MHz crystal, can a 16 MHz crystal be used instead?

I appreciate any assistance,

Cody