This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm working CC2538.
However, I have some confusion for designing because of the difference between CC2538-CC1200EM Reference Design and CC2538 datasheet.
There are some following issues. What's correct circuit?
1. The difference of RF matching circuit.
2. The difference of reset filter circuit's resistor.
The schematic drawings in the datasheet are always meant as an illustration. The reference design is always the correct one.
That said I found out that the CC2538 reference design is not on web, please see attached. 6428.CC2538EM_1_1_0.zip
Hello Se-Hee Whang,
The RF balun and matching circuit in the datasheet was taken from the CC2538EM reference design, which has an SMA connector and a PCB antenna in a "select one" configuration as follows:
It seems that this reference design has been replaced by another reference design on the CC2538 product page by mistake. We will fix this as soon as we can.
The CC2538+CC1200EM reference design is similar, but, as is often the case, has some component value tweaks to optimize performance on that particular board. As a starting point, you should always use the component values in the reference design that you are basing your own design on.
For the Reset_N filter, I recommend using 2.2kOhms. The 2.2 ohm value from the datasheet might be a typographic error, but this filter is optional (albeit recommended), so you will be able to choose quite freely in your own design.
I hope this helps.
-EWI