This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
this should give an idea of how to integrate your particular solution. You can place the SAW filter after the LNA/PA
http://www.ti.com/tool/cc112xsky65367em-rd
if you have a specific LNA/PA and SAW in mind let us know and we can suggest a configuration.
Thank you Farrukh. I am familiar with the link you sent me, but taking that approach (which is for 169MHz application) would require component value changes for my 420-470MHz application, plus an antenna switch which I'm hoping to avoid with CC112x. Can I send you a schematic?
Thanks. The attached schematic is from TI's reference design (CC112xEM_420_470). I've highlighted capacitor C181 which taps off RX signals at point A. Ideally (unless you suggest otherwise) I'd like to remove C181 pin 2 from point A and instead connect my LNA/SAW circuit to point A. Then C181 would be connected to the output of my LNA/SAW circuit. However, for this scheme to work the impedance at point A needs to be 50 ohms as my LNA/SAW circuit has 50 ohms in/out. Any thoughts? Alternative solutions would involve an antenna switch, and component value changes, both of which I'd like to avoid if I can.
Thanks
Ideally you could place the LNA where you have suggested and SAW instead of L173, C177, L174, and C175 to knock down harmonics.
I believe the impedance at point A is 50ohm but i will verify this with simulation and get back to you.
Thank you for the speedy replies.
Replacing the filter components with the SAW is a good idea, although the SAW then needs to handle the required TX power from CC112x.
It would be great to know if point A is already at 50 ohms.
Thanks.
I have attached the S11 file measured at point A by lifting L173 and setting the CC1120 in RX mode.
Now this includes the effect of L172 and C176 portions of the network. This will help you with impedance calculations.
Also, for your particular application, you may have to tweak the balun to have impedance looking into the LNA/SAW to be 50ohm. Please see this AN068 for reference.
!Agilent Technologies,E5071B,MY42301378,A.09.10 !Date: Mon Jan 27 10:56:58 2014 !Data & Calibration Information: !Freq S11:SOLT2(ON) # Hz S RI R 50 1000000 1.007842e+000 -3.018761e-002 8495000 9.794376e-001 -2.223932e-001 15990000 8.988328e-001 -3.995303e-001 23485000 7.813489e-001 -5.482725e-001 30980000 6.372680e-001 -6.600929e-001 38475000 4.786313e-001 -7.347236e-001 45970000 3.257477e-001 -7.691408e-001 53465000 1.814904e-001 -7.804286e-001 60960000 4.629389e-002 -7.650353e-001 68455000 -7.779147e-002 -7.319126e-001 75950000 -1.870427e-001 -6.846595e-001 83445000 -2.841654e-001 -6.242324e-001 90940000 -3.661583e-001 -5.559456e-001 98435000 -4.378267e-001 -4.793573e-001 105930000 -4.990920e-001 -3.939862e-001 113425000 -5.445066e-001 -3.008449e-001 120920000 -5.775430e-001 -2.054364e-001 128415000 -5.964366e-001 -1.110044e-001 135910000 -6.036824e-001 -1.833236e-002 143405000 -6.011330e-001 7.295605e-002 150900000 -5.881021e-001 1.617695e-001 158395000 -5.647467e-001 2.470435e-001 165890000 -5.312455e-001 3.253840e-001 173385000 -4.884129e-001 4.004427e-001 180880000 -4.357656e-001 4.708021e-001 188375000 -3.759391e-001 5.379769e-001 195870000 -3.104287e-001 5.888780e-001 203365000 -2.388480e-001 6.247313e-001 210860000 -1.618439e-001 6.536637e-001 218355000 -8.675141e-002 6.723324e-001 225850000 -8.974189e-003 6.831244e-001 233345000 6.843458e-002 6.833537e-001 240840000 1.440602e-001 6.767645e-001 248335000 2.160658e-001 6.617604e-001 255830000 2.840896e-001 6.390865e-001 263325000 3.460645e-001 6.075020e-001 270820000 4.050573e-001 5.677713e-001 278315000 4.616769e-001 5.222914e-001 285810000 5.125314e-001 4.729287e-001 293305000 5.547675e-001 4.207547e-001 300800000 5.888801e-001 3.626216e-001 308295000 6.159181e-001 2.985376e-001 315790000 6.379865e-001 2.310715e-001 323285000 6.502531e-001 1.620659e-001 330780000 6.542675e-001 9.172249e-002 338275000 6.484505e-001 2.099162e-002 345770000 6.307869e-001 -4.778258e-002 353265000 6.027022e-001 -1.124444e-001 360760000 5.622040e-001 -1.710058e-001 368255000 5.113984e-001 -2.171823e-001 375750000 4.615063e-001 -2.541952e-001 383245000 4.142667e-001 -2.941241e-001 390740000 3.566298e-001 -3.391435e-001 398235000 2.842529e-001 -3.740269e-001 405730000 2.010064e-001 -3.909288e-001 413225000 1.117949e-001 -3.827220e-001 420720000 2.647961e-002 -3.516100e-001 428215000 -4.879086e-002 -3.025658e-001 435710000 -1.081839e-001 -2.398557e-001 443205000 -1.495600e-001 -1.662975e-001 450700000 -1.730113e-001 -8.723126e-002 458195000 -1.766439e-001 -6.553512e-003 465690000 -1.621899e-001 6.961996e-002 473185000 -1.304597e-001 1.359967e-001 480680000 -8.741305e-002 1.909126e-001 488175000 -3.622605e-002 2.328851e-001 495670000 1.762499e-002 2.635397e-001 503165000 7.180017e-002 2.823422e-001 510660000 1.242918e-001 2.913006e-001 518155000 1.762402e-001 2.876118e-001 525650000 2.263408e-001 2.780850e-001 533145000 2.721791e-001 2.655717e-001 540640000 3.101192e-001 2.493837e-001 548135000 3.388125e-001 2.276192e-001 555630000 3.631035e-001 2.028248e-001 563125000 3.883331e-001 1.795810e-001 570620000 4.144656e-001 1.558527e-001 578115000 4.384317e-001 1.285384e-001 585610000 4.579000e-001 9.840369e-002 593105000 4.722568e-001 6.533107e-002 600600000 4.832729e-001 3.196577e-002 608095000 4.897862e-001 -3.481691e-003 615590000 4.909019e-001 -3.666215e-002 623085000 4.859049e-001 -7.072732e-002 630580000 4.773446e-001 -1.044817e-001 638075000 4.648002e-001 -1.357526e-001 645570000 4.516420e-001 -1.658454e-001 653065000 4.319958e-001 -1.890366e-001 660560000 4.040327e-001 -2.077566e-001 668055000 3.669744e-001 -2.246698e-001 675550000 3.264447e-001 -2.377809e-001 683045000 2.845800e-001 -2.387352e-001 690540000 2.407875e-001 -2.214204e-001 698035000 2.009844e-001 -1.861636e-001 705530000 1.766607e-001 -1.340979e-001 713025000 1.800154e-001 -7.272292e-002 720520000 2.174306e-001 -1.823407e-002 728015000 2.822662e-001 1.373893e-002 735510000 3.560008e-001 1.578245e-002 743005000 4.224425e-001 -8.951018e-003 750500000 4.737895e-001 -4.877276e-002 757995000 5.086948e-001 -9.584210e-002 765490000 5.306559e-001 -1.466346e-001 772985000 5.412595e-001 -1.911618e-001 780480000 5.417446e-001 -2.317316e-001 787975000 5.362782e-001 -2.685262e-001 795470000 5.278398e-001 -3.015678e-001 802965000 5.157453e-001 -3.331783e-001 810460000 5.018201e-001 -3.647934e-001 817955000 4.873858e-001 -3.914984e-001 825450000 4.713382e-001 -4.159916e-001 832945000 4.552017e-001 -4.395907e-001 840440000 4.391339e-001 -4.598970e-001 847935000 4.229283e-001 -4.793702e-001 855430000 4.073442e-001 -4.960679e-001 862925000 3.887538e-001 -5.093563e-001 870420000 3.716368e-001 -5.212362e-001 877915000 3.550534e-001 -5.329529e-001 885410000 3.540432e-001 -5.532765e-001 892905000 3.389667e-001 -5.627825e-001 900400000 3.222886e-001 -5.741426e-001 907895000 3.047238e-001 -5.835895e-001 915390000 2.862568e-001 -5.930636e-001 922885000 2.687077e-001 -6.009395e-001 930380000 2.519209e-001 -6.083554e-001 937875000 2.344602e-001 -6.124959e-001 945370000 2.150655e-001 -6.154478e-001 952865000 1.973219e-001 -6.196401e-001 960360000 1.800217e-001 -6.251374e-001 967855000 1.682732e-001 -6.291853e-001 975350000 1.584804e-001 -6.329920e-001 982845000 1.459393e-001 -6.343707e-001 990340000 1.321483e-001 -6.364620e-001 997835000 1.166278e-001 -6.390403e-001 1005330000 1.019080e-001 -6.408590e-001 1012825000 8.942946e-002 -6.427868e-001 1020320000 7.727289e-002 -6.421950e-001 1027815000 6.467434e-002 -6.430131e-001 1035310000 5.312757e-002 -6.433391e-001 1042805000 4.240543e-002 -6.433661e-001 1050300000 3.297438e-002 -6.415625e-001 1057795000 2.285930e-002 -6.410707e-001 1065290000 1.344756e-002 -6.398472e-001 1072785000 4.238346e-003 -6.395630e-001 1080280000 -7.409365e-003 -6.392074e-001 1087775000 -1.795186e-002 -6.374767e-001 1095270000 -3.027717e-002 -6.383291e-001 1102765000 -4.156180e-002 -6.401361e-001 1110260000 -5.277962e-002 -6.408040e-001 1117755000 -6.194143e-002 -6.397862e-001 1125250000 -6.989401e-002 -6.400067e-001 1132745000 -7.713530e-002 -6.414013e-001 1140240000 -8.385048e-002 -6.425828e-001 1147735000 -8.866252e-002 -6.423241e-001 1155230000 -9.586628e-002 -6.440939e-001 1162725000 -1.052673e-001 -6.455920e-001 1170220000 -1.136002e-001 -6.457345e-001 1177715000 -1.238168e-001 -6.453423e-001 1185210000 -1.341564e-001 -6.459491e-001 1192705000 -1.464338e-001 -6.483331e-001 1200200000 -1.584321e-001 -6.566872e-001 1207695000 -1.644602e-001 -6.607217e-001 1215190000 -1.714919e-001 -6.608551e-001 1222685000 -1.832431e-001 -6.588636e-001 1230180000 -1.984478e-001 -6.567244e-001 1237675000 -2.123578e-001 -6.588195e-001 1245170000 -2.245838e-001 -6.609159e-001 1252665000 -2.368790e-001 -6.611867e-001 1260160000 -2.472521e-001 -6.620909e-001 1267655000 -2.592491e-001 -6.621102e-001 1275150000 -2.726080e-001 -6.599914e-001 1282645000 -2.845990e-001 -6.574910e-001 1290140000 -2.945408e-001 -6.571488e-001 1297635000 -3.068871e-001 -6.539222e-001 1305130000 -3.200983e-001 -6.701902e-001 1312625000 -3.350713e-001 -6.645423e-001 1320120000 -3.505509e-001 -6.585349e-001 1327615000 -3.635382e-001 -6.515324e-001 1335110000 -3.772109e-001 -6.444973e-001 1342605000 -3.899686e-001 -6.390850e-001 1350100000 -4.020178e-001 -6.353947e-001 1357595000 -4.143854e-001 -6.322563e-001 1365090000 -4.276603e-001 -6.284030e-001 1372585000 -4.411410e-001 -6.237909e-001 1380080000 -4.526844e-001 -6.185533e-001 1387575000 -4.639767e-001 -6.113834e-001 1395070000 -4.739066e-001 -6.030308e-001 1402565000 -4.843223e-001 -5.914376e-001 1410060000 -4.949272e-001 -5.825582e-001 1417555000 -5.063346e-001 -5.719366e-001 1425050000 -5.164178e-001 -5.630565e-001 1432545000 -5.282720e-001 -5.541469e-001 1440040000 -5.394350e-001 -5.468517e-001 1447535000 -5.484637e-001 -5.388999e-001 1455030000 -5.595073e-001 -5.315796e-001 1462525000 -5.690326e-001 -5.226736e-001 1470020000 -5.780341e-001 -5.146892e-001 1477515000 -5.869369e-001 -5.063125e-001 1485010000 -5.945885e-001 -4.966533e-001 1492505000 -6.029553e-001 -4.878864e-001 1500000000 -6.134860e-001 -4.773476e-001