I am developing a product that will include a RF430CL330 as a NFC target for communications, however the other electronics in the target device will require contact-less power, which I aim to supply via an inductive charging field. It is my understanding that the inductive antenna can only input a maximum of 4.1v to the RF430. Is it possible to isolate the antenna from the chip? Ideally I would like to use both inductive power and NFC at the same time, effectively turning the target device into a higher-power passive NFC tag.