Dear Friends:
I had seup CC1020 for UART mode transmission. The receiver detect carrier. But what is very strange is that there is irrelevant data on DCLK which I have used as RX data even when transmitter is off.
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks you. If you would excuse me I have furthur questions!
1- I have an telemetry application for cc1021 in which output power should increase to 5w by external amplifier. Is it basically suitable for sucjh application?
2- I have made two cc1021 module with exactly the same components from reference design. programing two with the same frequency they are about 100KHz apart and can not be aligned with 3-10pf trimmer as in reference design!? Is it natural or something is wrong with my boards?