This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SmartRF Flash Programmer

When I try to launch the SmartRF Flash Programmer application, I get the error "This application has failed to start because the application configuration is incorrect.  Reinstalling the application may fix this problem." 

This is with Windows XP or in Windows XP mode on a Windows 7 machine.

The application opens on a Windows 7 machine, but it is the 64 bit OS so it does not recognize the USB port so I cannot use it.

Any help or suggestions is appreciated.

Thanks.