Hi,
with regards to TRF7962A PCD, we would appreciate that this would be given a high priority since it is a pressing matter to the customer.
We currently using TRF7962A to communicate with ISO/IEC 15693 tags, We've found that in most our tags, When we read the RSSI Levels and Oscillator Status Register, we get that the Auxiliary channel is higher considerably then the Main channel (4-12 dBm).
According to the datasheet there is an indiscrepancy about the Auxiliary channel description: on the one hand it is described "Only the main receiver is used for reception; the auxiliary receiver is used for signal quality monitoring."
On the other hand: "The MCU can read the RSSI values from the TRF7962A RSSI register and decide if swapping the input signals is preferable or not."
We've tried to use the Auxiliary channel by setting the Chip Status Control register, and even though we can see the changes made in the RSSI register, there is no physical change in the distance we are able to read the tag (should be greater according to the RSSI levels).
We've even shorted the main channel and still were able to read and write to Tag (The chip was set to use the main RX), so it seems that the RX came from the Auxiliary even though it was not set.
The question is, How can we use the Auxiliary channel, and can it be used for read and write commands? If so, Should we see a difference in distance we are able to read the Tag?
Please advise ASAP
BR,
Rotem