This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF7962A: TRF7962A Read Multiple Blocks Failure failure

Part Number: TRF7962A

I used TRF792A to read multiple blocks  and use read multiple blocks command(0x23) . I found that there was no problem in reading several blocks. When  read 28 blocks, TRF7962A can't read success。sometimes,  Call  inventory command, TRF7962A can't  inventory tags. when I reset  the hardware,TRF7962A work normally!

I try to read blocks separately, read 20 blocks first and then read 8 blocks , now I can read 28 blocks OK,However, there is a problem. TRF7962A will not work after  read 28 blocks continuously for a period of time.

At the same time, I went to test the detection EAS feature, and the same problem occurred,TRF7962A stopped working。

When TRF7962A cannot work properly, the MCU can work normally. Use oscilloscope to test TX pin  circuit waveform, The waveform is correct。

So I want to know how to solve this problem?