This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8530: NOT Paring

Part Number: CC8530

Hello,everyone! I had cc8530 chip headset design, but when I used RF data rate is 2Mbps, it can't be paring.But when used the 5Mbps, I done well.How to solve this issue. Attatch the config file. Thanks!T6.rar

  • Hi,

    Thank you for your interest in our Pure Path Wireless products.

    I wonder if the issue you are experiencing could be due to some configuration issues. Could you please verify one more time that both the master and the slave are properly configured?

    In the files you have provided, it seems that both the master and the slave are configured for 2 Mbps.

    Regards,

  • Thank you for your answer. Yes, only the 2Mbps or 5Mbps as difference. From the help file as follow described:  

    Radio and Network

    RF data rate
    Specify which RF data rate to use, 5 Mbps (default) or 2 Mbps. Note that networks using different RF data rates are incompatible (invisible to each other). The setting must be identical for protocol master and protocol slaves to be compatible.

    In most cases the default 5 Mbps data rate should be used. Using the 2 Mbps data rate increases sensitivity (and thereby theoretical range) at the expence of throughput capacity and number of tries per audio slice, and is only recommended for networks with:

    • 1 audio channel using any streaming format or 2 audio channels using the SLAC or PCMLF streaming formats
    • Maximum audio latency (2048 samples)
    • Maximum slave count of 1