Other Parts Discussed in Thread: TAS2562, , TAS2562S
I am testing a new prototype board with the cc8530 on it. It is a network slave driving two tas2562 amplifiers. I have been able to load the software onto it, but when trying to use the power button it will very briefly turn on (I see a spike in current draw for about half a second) then immediately shut back off. I changed in the software to have it not require a power button, in which case it seemingly turns on and the LED indicator displays the alone LED pattern, but when I press the pairing button the LED pattern does not change. So, I cannot get the board into pairing mode. I have not tuned the antenna on this board or the network master board yet, so I am unsure if they would even be able to pair if it did work. Why would neither of these buttons work?
Thank you,
Austin