Part Number: WILINK-BT_WIFI-WIRELESS_TOOLS
Tool/software: Linux
Hi,
I am using WL1837 module in a IMX6 based custom device. The device has Android Oreo. Bluetooth is up and running and I can able to connect with BT devices.
As part of compliance testing, I am porting SS1BTPM and SS1Tool and try to run on this device. I have run the pre-built binaries present in AM335xBluetopiaLinuxProduction-4.0.3.0.1.0-linux-x64-installer.run and SS1BTPM is immediately exit with error value 220. There is no error messages and so I have no idea what is the reason for the error.
When run the SS1Tool, it exit with the message "Bluetopia Platform Manager service cannot be found. Exiting.".
I have build both these binaries using the toolchain in ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin but this also have the same result, exit with error code 220.
Could you please tell me what is the reason for this problem and how can I proceed with porting SS1BTPM and SS1Tool?
Regards,
Pratheesh