Part Number: CC8520
Other Parts Discussed in Thread: TLV320AIC3101
Hi
i am using the cc8520 with the tlv320aic3101 , and for project i have used one of the example of Pure path Wireless Configurator , and also i have used the Autonomous mode , the project that i have used is Preloaded Demo of the CC85XXDK , my cc8520 have the MCLK , BCLK , WCLK for the audio codec and also in the master i have the i2s data on the DOUT Pin , but at the slave i have no data on the DIN Pin and also the impedance of this pin to ground is about 100 ohm when master and slave have been paired , the slave and master paired to each other successfully and i have check this with the led pattern , and also the led pattern work in the active mode , with checking the board i am sure that the master and slave have communication with each other because when i change the FS at the master , the slave detect it and change the FS Clock to one that i have Choose at the master side , but with all of the state that i explained i have no data at the Din Pin of the Slave and so i have no audio , anyone can help me to resolve this ?
thanks