Other Parts Discussed in Thread: TRF7970A
I'm looking for some help designing a custom electronic hexagon game board. The game is fully developed, but I'm still prototyping the electronics portion. Each hexagon cell side is 1 inch. The board is also a hexagon, with 11 cells per side. There are a total of 331 cells. 18 of which are unused. So that means there are 313 usable cells. The dividing lines between cells is about 1/16 inch wide. I'm using https://smile.amazon.com/gp/product/B07MKWHYQK/ (ntag215) to identify the game pieces. There are 36 kinds of pieces.
I liked the article http://www.ti.com/lit/an/sloa167/sloa167.pdf to describe how to multiplex out to 16, but obviously I need to go a lot further. For ease of construction, I'd like to use a pcb trace for my "antennas" (Yes, I know this isn't the proper term) as described in http://www.ti.com/lit/an/sloa135a/sloa135a.pdf. I did read over the http://www.ti.com/lit/an/sloa231/sloa231.pdf report that suggests using the TRF7970A reader.
I know there will be a trade off in speed verses cost if I only use one reader chip. My thought was design the game board in slices of 52 cells per circuit board, with one reader per slice. One circuit board would have 53 cells, to include the center cell of game board.
Part of the challenge is that I need a LED in the middle of each cell. The board will be covered with a sheet of acrylic (1/8 - 1/4 inch... not sure yet). I would like the antennas to be hexagon in shape. I'm only looking for a read distance of around 1/2 in. My bigger concern is not getting readings from other nearby cells. Could I use a 2 sided PCB? one side for the antennas, and the other side for all the antenna switching & LED control? If I can't use a double sided PCB due to interference problems, how much separation do I need?
Any guidance would be appreciated.