Other Parts Discussed in Thread: CC2640R2F, CC2571, CC2511
Goodmorning,
we are looking for a transceiver device to develop a system with one receiver and some transmitters (up to 5 transmitters) to be used in Health/fitness. Each transmitter has the role to send data of sensors and monitor devices to the single receiver which is a USB dongle plugged into a PC. The idea is that all the sensor devices, that are acquiring different data, are paired in a fixed way with a single receiver which is collecting data from sensors and send them to the PC over USB.
Each sensor send a new value (5 byte) every 10ms, so the receiver needs to be fast enought to receive them.
All the sensor devices (transmitters) must be movable. All the system is intended to be used indoor (in a single room) or outdoor.
All the devices has to be as small as possible, so it's better if we use PCB antennas.
The reason we found the CC2500 device is because of the Proprietary 2.4 GHz that probably allow us to develop a system which is away from issue relating to common Bluetooth pairing for the end user. So it will be plug and play without configurations for the end user.
Is this device suitable for the application we need? Is there any better solution?
Thanks.
Is this device suitable for the application we need?