Hello!
I have a board with STM32F777 MCU and TRF7960A chip connected via SPI with 1.875 MHz frequency.
Chip is initialized using sloa227b library according to the specific of the trf7960A chip. I can read and write data to registers, for example I changed Bits 4 & 5 of the 0x09 register and saw with the oscilloscope the frequencies 13.6, 6.8, 3.4 & 0 MHz on the SYS_CLK pin.
But on TX_OUT pin the carrier signal is presented even if bit 5 in 0x00 register is set to zero, which means that transmitter is off. What can be the problem?
Best regards