Hi,
I am looking for devices that covers the 385.5MHz frequency band and I saw below thread.
The CC1352R is recommended, but this is not clear.
The CC1352R supports below frequency bands. It supports 359MHz, but the 358.5 MHz is not in the band.
143-176, 287-351, 359-439, 431-527, 861-1054, 1076-1315, 2360-2500 MHz
However, the frequency of the receiver to be developed by the customer is 358.5000 MHz ± 500 Hz.
Does the CC1352R support 358.5000 MHz? If this is not possible, please recommend another part.
I found it, but it wasn't in TI sub 1GHz products.