Other Parts Discussed in Thread: SYSCONFIG
Hi,
Sorry if this has already been answered, but I can't find a concise description of what I need to do.
I am about to start compliance testing (EN 300 220) and need to set up an unmodulated and modulated test signal for my CC1312R on a custom board which is representative of the Simplelink 5kbps long-range mode. Can you confirm this is a good way to do this please?
1) I'm using IAR so I can start with the rfCarrierWave rtos example (not sure if rtos vs nortos makes any difference here): C:\ti\simplelink_cc13x2_26x2_sdk_4_30_00_54\examples\rtos\CC1312R1_LAUNCHXL\drivers\rfCarrierWave
2) Then using Sysconfig I can change the radio configuration to 5kbps long-range mode and set rf channels appropriately. No need to use RF Studio at all.
3) I can configure the carrier to be modulated or unmodulated in the C code.
4) Download the code so it runs without any debugger attached.
Many thanks,
Andy