Hello,
I have a problem that with TI15.4 STACK, Beacon MODE, some times sensor will loss 4 beacons. But I checked the RSSI signal, it is good!
I route out LNA active pin to gpio. And I find that in sensor side, the beacon receive windown is about 10.4ms。
As I add some data to COP beacon payload, now the length of beacon is 85 bytes (confirmed by sniffer). The rate is 50kbps.
so it need (85*8)/(50*1024) = 13.28125ms to send the bytes.
But in the sensor side ,it only have 10.4ms beacon receive window, Is it the problem??
So, How can I modify the beacon recieve windows on sensor side?
Here is the relate setting of my project:
#define CONFIG_MAC_BEACON_ORDER 4
#define CONFIG_MAC_SUPERFRAME_ORDER 4
#define CONFIG_RX_ON_IDLE false
Many thanks!
Jun