Hi, TI.
I find that in simplelink_cc13xx_cc26xx_sdk_6_10_00_29, there is uart2 driver example but not uart example as below:
So, I want ask, is uart (not uart2) unavailable in SDK v6.10?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI.
I find that in simplelink_cc13xx_cc26xx_sdk_6_10_00_29, there is uart2 driver example but not uart example as below:
So, I want ask, is uart (not uart2) unavailable in SDK v6.10?
Hi yingtao,
The UART example has been deprecated in the SDK version 5.30 in favor of the UART2 examples.
However, the source for the UART driver is still available in the Simplelink SDK v6.10 but this will also be deprecated and it will not be available in SDK v6.20.
So the recommendation is to use the UART2 driver.
It is mentioned in the upgrade and compatibility information of the CoreSDK.
Regards,
Sid