HI TI.
I'm using CCS V12 with simplelink_cc13xx_cc26xx_sdk_6_20_00_29.
how can I import the CC1311 sample code?
I can't find a sample code for CC1311.
could you help me?
I have a CC1312 program that needs to be ported to CC1311,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI TI.
I'm using CCS V12 with simplelink_cc13xx_cc26xx_sdk_6_20_00_29.
how can I import the CC1311 sample code?
I can't find a sample code for CC1311.
could you help me?
I have a CC1312 program that needs to be ported to CC1311,
Please try to do the following steps:
Start with one of the examples for the CC1312 from the SDK and switch the device to CC1311R3RKP
Change the device family from DeviceFamily_CC13X2X7 to DeviceFamily_CC13X1
Under project settings -> Build -> Arm Compiler -> Processor Options view, change
Under project settings -> Build -> Arm Linker -> File Search Path -> Include library file or command file as input.
Replace:
ti/devices/cc13x2x7_cc26x2x7/driverlib/bin/ticlang/driverlib.lib
with:
ti/devices/cc13x1_cc26x1/driverlib/bin/ticlang/driverlib.lib
Remove the CC13x2x7 linker file (cc13x2x7_cc26x2x7_xxx.cmd) from the project and replace it with the correct CC13x1 linker file (cc13x1_cc26x1_xxx.cmd) found here:
C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\source\ti\boards\cc13x1_cc26x1
HI Expert.
Thank you very much for your help, I can use it already,
I think this thread will be very helpful for other people later.