Other Parts Discussed in Thread: CC1310, , CC2652P7, CC2652R
Hello,
We are porting a CC1310 design to a CC1352P7 design. I am not able to get the device into STANDBY. As you can see below I am printing out data just prior to us doing a semaphore_Post operation which should allow the system to take advantage of STANDBY. There is only 1 constraint (#2 which disallow standby shown below) which is due to the serial port being active. Post printing of this message, I release the UART and the last statements just prior to posting the Semaphore to be awaken on a push button, I check the status of "if(PowerCC26X2_module.constraintCounts[2])" is set, then I'll turn on a LED. The LED is off, so it should be OK for the Power Policy (standard one) to take advantage of STANDBY.
I'm drawing around 2 mA and I'm sure that other parts of my system will not use 2 mA of current. Any thoughts/comments welcome.
Thank you,
Shawn
*********************************************************
Power_getConstraintsMask = 4
Power_getPerformanceLevel = 0
Power_getTransitionState = 1
Power_getDependencyCount[0] = 0x0
Power_getDependencyCount[1] = 0x0
Power_getDependencyCount[2] = 0x0
Power_getDependencyCount[3] = 0x0
Power_getDependencyCount[4] = 0x0
Power_getDependencyCount[5] = 0x1
Power_getDependencyCount[6] = 0x0
Power_getDependencyCount[7] = 0x0
Power_getDependencyCount[8] = 0x1
Power_getDependencyCount[9] = 0x0
Power_getDependencyCount[10] = 0x0
Power_getDependencyCount[11] = 0x0
Power_getDependencyCount[12] = 0x0
Power_getDependencyCount[13] = 0x1
Power_getDependencyCount[14] = 0x1
Power_getDependencyCount[15] = 0x1
Power_getDependencyCount[16] = 0x0
Power_getDependencyCount[17] = 0x0
Power_getDependencyCount[18] = 0x0
Power_getDependencyCount[19] = 0x0
Power_getDependencyCount[20] = 0x0
Power Constraint Count[0] = 0
Power Constraint Count[1] = 0
Power Constraint Count[2] = 1
Power Constraint Count[3] = 0
Power Constraint Count[4] = 0
Power Constraint Count[5] = 0
Power Constraint Count[6] = 0
Entering deep sleep (S)