This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125: Problem with data transmission using CC1125.

Part Number: CC1125

I have a custom PCB with a microcontroller and a CC1125. Operating parameters - Frequency 169MHz. Deviation 3kHz. Modulation 2GFSK. Symbol rate 12ksps. Packet mode. Transmit only. 

CC1125 Version 0x21     TXCO 38.4MHz.CC1125.pdf

I have two Smart RF transceiver evaluation boards 'TrxEB" and two 169MHz RF modules. One of the modules was configured to transmit using the above settings and the other RF module was configured to receive the frames. This was successful.

I then used the Smart RF Studio settings for the RF transmitter module on the custom board. I modified some of the settings to suit the 38.4MHz TXCO on the custom board.

I then disconnected the RF transmitter module and connected the RF receiver module to the custom transmitter board. 

On the custom board, I am able to configure the CC1125 correctly for frequency and power. However, I am not able to transmit data. The attached spectrum analyser plot shows the RF spectrum being output from the custom board. There appears to be no modulation. Also, when connected to the Smart RF RF receiver module, there is no data reception. The Smart RF RF receiver module is receiving sufficient RF power from the custom board.

I have implemented the errata. 

Also attached is a screen shot of the SmartRF STudio receiver settings and the relevant source code for the custom board.

Can you think of any reason why there appears to be no data modulation ?

Why does the SmartStudio RF module not correctly receive the frames ?