This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I tried to read flash memory from CC1311 using the evaluation board (LP-CC1311P3). The evaluation board includes the USB debug probe XDS110.
First step I used the on-board jumpers and configured the as following:
Power_XDS110, GND, 5V, 3V3, Line_TMS and Line_TCK.
I read successfully the flash memory using UniFlash software GUI.
Second step I tried to connect 2 evaluation boards back-to-back, so in the first board I use as XDS110 debug probe only and in the second board I use CC1311 chip with its peripheral.
Connected lines/signals:
First board: power jumper disconnected
Second board: power jumper connected as Extern_Power.
Between boards connection: GND->GND, 5V->5V, 3V3->3V3, Line_TMS->Line_TMS, Line_TCK->Line_TCK.
XDS110 connection was success but when I try to read flash memory, I got the error: "[ERROR] IcePick_C: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.11.0.00128)"
What may be the reason for this error?
Note: UniFlash app. version: 8.3.0.4307
Thanks,
Alex Katsovich
Hi Alex,
In the first board you should connect the power jumper to XDS110 power.
Hi Diego,
I think I found the reason, should connect also RST_Line (Reset). Will test this.
Regards,
Alex