This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PUREPATH-WL-CFG: CC85xx USB not recognized/fail to enumerate: Unknown USB device

Part Number: PUREPATH-WL-CFG

Hi folks

Trying to use CC85xx EVK as USB audio hub using design example. USB not recognized on PC, after reinstalling PP-WL-CFG too. This is the message from Device Manager:

Windows has stopped this device because it has reported problems. (Code 43)

A request for the USB device descriptor failed.

I manually tried to reinstall the USB device from Program Files/Texas Instruments/USB Audio Device Driver/setup.exe . This does not complete because it looks for "vendor.cer" .

Help?

Note: I also run PP Configurator 2 and 3 on the same PC . I use the CC85xx to connect a TAS5754 setup in stereo 2.1 mode with the Line in input  via ADC on the EVK so far, but want to use USB please.