Hi folks
Trying to use CC85xx EVK as USB audio hub using design example. USB not recognized on PC, after reinstalling PP-WL-CFG too. This is the message from Device Manager:
Windows has stopped this device because it has reported problems. (Code 43)
A request for the USB device descriptor failed.
I manually tried to reinstall the USB device from Program Files/Texas Instruments/USB Audio Device Driver/setup.exe . This does not complete because it looks for "vendor.cer" .
Help?
Note: I also run PP Configurator 2 and 3 on the same PC . I use the CC85xx to connect a TAS5754 setup in stereo 2.1 mode with the Line in input via ADC on the EVK so far, but want to use USB please.