Hello, thank you for viewing my question.
i am implementing a fire detection system with firmware update (ota) enabled.
i am trying to implement oad using RF(447Mhz) - not BLE
before registering this question, I implemented it according to the instructions in the link below.
(TI 15.4-Stack - Over the Air Download (OAD)) --- (A)
(TI 15.4-Stack - Linux Gateway Project Zero) --- (B)
the example code used is as follows:
client : bim_offchip
server : coprocessor
while implementing according to (A) and (B), when I entered the command to run the gateway, the output was different from the expected result. I found out that the examples (A) and (B) were based on CC13x2 & CC26x2, and I thought that the cc1350 I use should be implemented in a different way.
how can I do OTA from CC1350 to RF?(not BLE)
i am looking for examples and advice on implementation.
is only BLE-based OTA possible with the cc1350?