Other Parts Discussed in Thread: CC1312R, , CC1310
Hi,
According to my test it looks that the power detector not measuring correctly the RSSI value, on 433MHz band. The reported RSSI value is about 5-6dB higher than the signal itself.
This problem does not exist on 868 or 915MHz
I checked it on my PCB and on your launch pad while the CC1312R and CC1312R7. using as transmitter and receiver.
As you can see in the table below on the 433MHz for example the transmitted signal is -67.5dBm (measured by spectrum analyzer) and the Get RSSI indicate -61.5dBm (by the smart RF studio)
On the 915MHz the RSSI level is similar to the power of the transmitted signal.
Band | CC1312R7 as Tx | CC1312R as Rx | CC1312R as Tx | CC1312R7 as Rx |
915 | -60 | -59 | -64 | -65 |
433 | -32.5 | -27 | -67.5 | -61.5 |
Thanks,
Shamai Yossi