Other Parts Discussed in Thread: CC1190,
Hi there,
In our custom design based on CC1354P10RGZ, we are using this crystal with external load capacitor mounted, and it's properties are well within the other similar crystal which TI suggest.
So i would like to know -
- Does above crystal fine to use? as long as it is matching the design/layout rules ?
- We see that CC1352P10RGZ works fine (except the RF), On RF still we in Testing mode as we use it with External PA CC1190, but i would like to know do we required to disable internal load capacitance? (if yes then how do that in Smart RF Studio?)
- Generically i would like to know the performance of the RF vs crystal used? (let's say if tolerance is bad or due to pcb/design issue crystal's performance is bad), in this situation , will output of RF(SubGHZ or 2.4Ghz) will be totally off? or it will be degraded. Ex. If we set transmit power to 5dbm and can get around 0 dbm signal because of crystal's behavior?
Regards,
The Mat