Tool/software:
Hello,
I have some questions regarding the CC1200 at 868MHz:
- In the CC1200 datasheet, Table 4.1 shows that the maximum voltage on the analog pin is 2V. However, when we supply 3.3V as per application note (SWRR121), the DC voltage at Pin 17 (PA) is 2.7V because of the R171 (10 ohms) (basic voltage divider rule). Is that correct?
- The above calculate is under the assumption that Pin 17 internal load impedance is 50 ohms, is this assumption correct?
-
Can I use different supply voltages, for example, 3.3V for all analog pins (i.e., Pin 17) and 3V for all digital pins (i.e., Pins 12, 5,1,13,15, etc.)?
-
In the CC1200 datasheet, Table 4.14 shows the load capacitance for the crystal oscillator as 10pF. However, in application note (SWRR121), it is 15pF. Which of them is the correct value?