Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Sorry to ask, perhaps obvious to some...
I try to add a SPI device to my CC1312 board in making. I get the suggestion to use the following pins
SCLK 16/32
POCI 15/11
PICO 12/19
CSN 1/30
Why are there two pin suggestions, and how do I select between the two?
POCI, pin 15 is used for backdoor programming, but I can change that
CSN pin 1 is used for UART_1, so that is a conflict.
I can see that I can select other pins, but they are always shown as a pair?
Best Regards,
Gullik