Other Parts Discussed in Thread: CC1120, BOOSTXL-CC1120-90
Tool/software:
Hi,
I'm a little bewildered to why I'm not seeing any gain on a new design using the CC1190 PA/LNA following a CC1120 transceiver.
Essentially, testing with a CW carrier at 868MHz, the expected output from the PA is over 26dBm, whereas I'm only measuring just under 0dBm ?!?
Thinking it could something on the CC1120 transceiver side, I decided to remove that stage from the circuit by removing a 10nH inductor from the LC matching on the SAW filter output, going into the CC1190 input port, and added a signal from a tracking generator on the SA at this input just to see where the gain is lacking on my radio.
The result is, with -20dBm TG signal input all I'm seeing on the CC1190 output is a signal slightly below -20dBm ?!? So essentially getting the TG signal going straight through the CC1190, no gain, zilch... if anything a slight loss of about 1dB from input to the SMA output ?
This is unexpected as the CC1190 design is based on a TI reference design schematic with identical components (albeit a variation on the routing and stack-up) that we have used before in a 99% same configuration.
I've checked the HGM pin and it's at +3.3V, the PA port is also high, and the PA power rails all check out fine at +3.6V. So, even if the assembly house botched up part (or two) of the output impedance match slightly (for whatever reason, but I doubt it as they are a reputable PCBA), I would expect to see some gain, say with at most 3 - 4 dB penalty on output power at most, but still having an output over +20dBm with +7dBm input power.
Just wondering what might have caused this (or could cause it) and should I be worried the CC1190 was deep-fried during assembly or is this unlikely ? no other issues on the PCB otherwise, all good and other PCB digital and analogue tests pass with flying colours, just the CC1190 gain being 0dB is a real bummer ! Tests so far on 3 boards, identical issue, no gain !
With the PA on, the current drawn is about 100mA at +4,2V supply input. I was expecting more current drawn also, if the output were closer to +27dBm maximum.
Any other possible checks I could do on the CC1190, other than replacing the device with a new one, as a last resort ?
Any thoughts, advice, suggestions would be appreciated...
Regards, MM