We are using a Cc1190 to boost the output of a 1GHz transceiver. We power via USB C and a 3.3V LDO. The issue we have is that we get profound sidebands above +18dB power output. we are using a 4 layer board as per the application notes. we are drawing approx 280mA from the power supply so approx 240mA is going to the CC1190.
The measurements are being made using a Tektronix RSA306B and we are using an inline 30dB antennuator, as we have observed similiar effects if we feed directly to the Spectrum analyser due to the input saturating.
The test is made by continuously driving the CC1190.
I have attached 2 plots, the effect seems to be evident from power level 5 and above.