Other Parts Discussed in Thread: CC2642R, UNIFLASH
Tool/software:
WSmartRFFlashProgrammer2.pdfhen I plugged in the XDS110 Debug Probe programmer, in SmartRF Flash Programmer 2 I see the XDS110, XDS-0000000 and underneath it shows Unknown until I refresh it a few times then it detects a CC2642R instead of my CC1213PSIP. There is also another XDS110 Class Application entry which I can change the Unknown listed to the correct Target Device. But this won't allow me to program anything. I also cannot use the Debug in my project for my custom board. Someone said that it may be a timing issue since SmartRF Flash Programmer 2 always works. Is there a reason why I see two devices in the app? What setting specifically do I need to change to get the debugging in CCS working?
Kevin