Tool/software:
I am unable to debug my project due to this error when it starts up the radio code. I see in the ti15_4stack directory for the sensor project that some of the path is there, but not the mac_radio.c. Is there a way to get the source to this or see what is actually causing the problem. When I run it normally, it doesn't get this error.
Can't find a source file at "/home/developer/.conan/data/ti154stack/6.41.00.07/librarylprf/ga/build/c90184d484f3f95c6a6179391966efa64b8ab8fe/build/cmake/ticlang/..\..\..\source\ti\ti154stack\low_level\cc13xx\mac_radio.c"
Locate the file or edit the source lookup path to include its location.
Thanks,
Kevin