Hi all,
I am working on a UNB project as part of my school paper and have not really much experience in microcontroller
programming but with a little understanding on wireless communication. So basically I am starting from scratch.
I just got this CC1125DK kit and had tried the smartRF studio working when connecting directly both the evaluation
boards working /communicating. However when i connect the MSP debugger interface in between, error came up
even after updating all the devices' firmware to current versions as prompted when i initially opened the apps.
Attached are screen shots of the two errors when opening the device controller panel either with SmartRF studio or
SmartRF flash Programmer.
Note that :
1) I have powered off the evaluation board as I noticed it wont get recognized when its ON .
2) I kept the switches at ENABLE and UART mode as I understood from the CC1125DK quick start guide .
The reason why I am doing is because I wanted a couple of things to try:
1) Make the on-board sensors running by making or loading the 'preset' codes
2) Bypass the microcontroller and just use the transceiver side only and let an arduino-connected sensor
as the I/O device instead.
I am not sure if what I am doing to get what i need make sense. So I would appreciate any help.
thanks
ariel