This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C1200 Continuous TX

Other Parts Discussed in Thread: CC1200

Hi,

I'm trying to implement continuous TX using CC1200 module. Based on the User Guide and SmartRF Studio, so far I have found two approaches to do so:

1) Continuous TX with synchronous serial mode: Feed a single byte repeatedly over GPIO using a two-wire serial interface (instead of SPI).

2) Continuous TX with random mode and infinite packet length: Transmit a continuous pulse using Random Mode. This way, we transmit dummy bytes (generated by PN9 generator) by sending only a STX command to the CC1200.

Is there any other way to implement continuous transmission using CC1200?

I would appreciate any help regarding this issue.

  • Since you are asking for other methods of continuously transmission it sounds like you are looking for a functionality not covered in 1) or 2).

    If so, what do you want to do? Please elaborate.

  • If you want a continuous unmodulated carrier set CFM_DATA_CFG = 0x1.

    Easiest is to use SmartRF Studio. Select "Continuous TX "tab and then select between "modulated" (with data format = random mode) or "unmodulated".

  • Thanks for your answers. I'm trying to prepare the module for FCC testing, because of that I wanted to know all the options and choose the best one for that purpose. I know that I have to use an unmodulated signal (as Sverre suggested). 

    Is there any specific approach you recommend for FCC test? I appreciate your help.

  • For FCC testing you need:

    - To send a CW. Only one register is needed to set for this.

    - Sending random data. Option 2 in your first post is the recommended way.