This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm trying to implement continuous TX using CC1200 module. Based on the User Guide and SmartRF Studio, so far I have found two approaches to do so:
1) Continuous TX with synchronous serial mode: Feed a single byte repeatedly over GPIO using a two-wire serial interface (instead of SPI).
2) Continuous TX with random mode and infinite packet length: Transmit a continuous pulse using Random Mode. This way, we transmit dummy bytes (generated by PN9 generator) by sending only a STX command to the CC1200.
Is there any other way to implement continuous transmission using CC1200?
I would appreciate any help regarding this issue.
Thanks for your answers. I'm trying to prepare the module for FCC testing, because of that I wanted to know all the options and choose the best one for that purpose. I know that I have to use an unmodulated signal (as Sverre suggested).
Is there any specific approach you recommend for FCC test? I appreciate your help.