This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I meet the problem as well. And I want to know if it will influence the function when I export the code to the software used the 5kbps. Now I meet the problem is that when I enable 20 Node deceives(packet length is 127). They are easy to block in the EasyLink_transmit all the time. Even though I call the EasyLink_abort to stop it, It does not effect.