Other Parts Discussed in Thread: TIDA-01002, CC3220SF
Hi,
Stumbled on another step of the TIDA-01002 demo: 3.2.1.1.9.1 "Using the SimpleLink Starter Pro App". All steps work as described until step 13...
13) Click the open button on the dashboard to allow sensors to join the network.
I go to my IBM Cloud Foundry App URL but there is no "open" button. When I refresh the page the open button is displayed for less than 1 second then disappears. I think the co-processor is not talking to the CC3220SF. I've run out of ideas... help!
Hardware on hand:
- 2x CC1352R1 LauchXL pcb rev B
- 1x CC1312R1 LaunchXL pcb rev D
- 1x CC3220SF LaunchXL.rev A
Have tried different combinations of above PCBs, loading prebulit files from TIDA01002 git and also compiling from source and tweaking UART pin assignments. No luck.
Below is typical terminal output from CC3220SF:
[Cloud GET Handler] Payload: {"ipAddress": "192.168.1.11", "wifiConnection": 1, "mqttConnection": 1}
[Link local task] Metadata Sent, len = 48
[Link local task] Data Sent, len = 71
[NWK GET Handler] Callback Called:
[NWK GET Handler] Metadata Sent; , len = 48
[NWK GET Handler] Data Sent: [Dev GET Handler] Callback Called:
[Dev GET Handler] Dev Data: [Link local task] Metadata Sent, len = 48
[Link local task] Data Sent, len = 0
[Cloud GET Handler] Callback Called:
[Cloud GET Handler] Payload: {"ipAddress": "192.168.1.11", "wifiConnection": 1, "mqttConnection": 1}
[Link local task] Metadata Sent, len = 48
[Link local task] Data Sent, len = 71
C: Net 1, Sending Ping request [639]
C: FH-B1 0xc0 to net 1, Sent (2 Bytes) [@ 639]
C: Rcvd msg Fix-Hdr (Byte1) 0xd0 from net 1 [@ 640]
C: Msg w/ ID 0x0000, processing status: Good