Other Parts Discussed in Thread: CC1310
Hi,
I bought the the CC1111EMK868-915 dongle to use for bands at 868MHz and 915MHz, and I saw the CC1111EMK868-915 description states that the dongle operates in the 868 MHz and 915 MHz frequency bands, but the board uses the 868Mhz chip antenna. I just wonder how it would work for the 916MHz if the chip antenna range is 858 - 878 Mhz. Are there 2 different CC1111EMK dongles that work at 868 and 915MHz? Thanks.