Hi,
I don’t know the details of MAGN_TARGET which is one of the AGC control parameters. How does it work, if MAGN_TARGET=3 (33dB) is selected?
Regards,
Sinsan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eirik,
Thank you for your reply. Noted that the MAGN_TERGET value controls the signal power level into the demodulator.
For example, if MAGN_TERGET=3 (33dB) is selected, will the demodulator input power be maintained at 33dB as shown in the attached file (How MAGN_TARGET works.pdf)? Furthermore, is the value 33dB the ratio of the antenna input to the demodulator input power?
Best regards,
Sinsan