Hi,
My customer is testing LAUNCHXL-CC1352R1. Firstly they want to run example application in SimpleLink CC13X2 SDK. They have two LAUNCHXL-CC1352R1, they want to run one of it as collector, and another one as sensor, however they found they cannot make the two EVMs connected. I noted in our "SimpleLink CC13X2 TI 15.4 Stack user's guide" there is a notification said:
To enable back-to-back transmissions from a device to the collector, the following configurations must be set:
- CERTIFICATION_TEST_MODE = true
- CONFIG_FH_ENABLE = true
However engineer told me these two configuration cannot be modified. They tried to modified the two configurations from 'false' to true, however it was changed back to 'false' automatically by ccs after they build the application. Why? How should they make the example application run?
Thank you!
John