Part Number: TI-15.4-STACK-GATEWAY-LINUX-SDK
Tool/software: Linux
Hi,
We are trying to port our system to the latest TI-15.4-STACK-GATEWAY-LINUX-SDK version (2.04.00.19) on a BBB. Compiling works but I get the following error on starting the collector:
0.014: ERROR: collector.cfg:295: [application] config-min-backoff not handled
0.014: ERROR: collector.cfg:295: Error: not-handled
0.015: Failed to read cfg file
Also tried the original non modified gateway sdk, but get the same error. If I comment the new config parameters the collector starts fine.
; Minimum MAC Backoff Exponent
;config-min-backoff = 3
; Maximum MAC Backoff Exponent
;config-max-backoff = 5
; Maximum CSMA Backoff
;config-max-csma-backoff = 4
; Maximum Frame Retries
;config-max-retries = 3
But these config parameters are to fix the issue with orphan nodes so I think we need them. I can see the parameters in linux_main.c
./collector/collector.cfg: config-min-backoff = 3
./collector/linux_main.c: if(INI_itemMatches(pINI, NULL, "config-min-backoff"))