Other Parts Discussed in Thread: CC1190
I have a custom, CC1101/CC1190, 869.525 MHz board and I'm using the NDK NX3225GA 27MHz crystal, same as the one in the TI CC1101-CC1190 869 EVM. The crystal has a +/-20ppm tolerance, +/- 30ppm over temperature.
With FREQ2, FREQ1, FREQ0 set to 0x203462, the CC1101 center frequency should be 869.525 MHz.
The measured center frequency has consistently been 869.46x MHz. Multiple boards, two testing companies. Calculation with a 20ppm 27MHz crystal set the range to 869.507 to 869.54.
Fcarrier = (Fosc / 2^16) * FREQ
The question is what would be the best way to address this and get the center frequency back to 869.525 in production? Modify the FREQ2..0 values in an after production test, or am I missing something?
Thanks for for your time!
-Rich