Hi,
I am using some code form no-Rtos LEDs and buttons example.
Custom board in Configsys.
I am trying to read 6 buttons. 5 buttons work well. When I add the 6th one, it does not work. Callback on the 6th is ignored.
I have increased number of buttons in #define to 6 or 7 - no luck.
If I comment out oppening of any one of 6 buttons all the other 5 work well, including my number 6 .
Is there some limit for the number of buttons in the Button library? If yes, how can I change it?
I did appreciated the simple access this library provides to clicks, double clicks etc.
Thanks,
Regards ,
Edward.