It seems the current version, SmartRF Studio 7, doesn't support the CC1070 - I need SmartRF Studio 6.
So I downloaded & installed Setup_SmartRF_Studio_6.13.1.exe
But when I run it and select CC1070, I get:
This is on Win7-Pro, 64-bit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It seems the current version, SmartRF Studio 7, doesn't support the CC1070 - I need SmartRF Studio 6.
So I downloaded & installed Setup_SmartRF_Studio_6.13.1.exe
But when I run it and select CC1070, I get:
This is on Win7-Pro, 64-bit.
We have to look into this. The issue is probably driver to parallel port driver. I get the same error if I try to start SmartRF Studio 6 in my PC.
I assume that this is related to https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/876905? Is it possible for us to help you in some way without getting SmartRF Studio 6 up and running? If this is related to the case I referred to I assume that you don't need to find settings for CC1070 as such but more as an input to he code conversion?
TER said:I assume that this is related to https://e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/876905?
Yes, it is.
TER said:Is it possible for us to help you in some way without getting SmartRF Studio 6 up and running?
The current code has settings just as a load of "Magic Numbers" - I just was hoping to use SmartRF Studio 6 to decode them ...
Thanks.
The numbers are
{ 0x0F, 0xF0, 0x8F, 0x3D, 0x70, 0x23, 0x39, 0x3D, 0x70, 0x23, 0x39, 0x44, 0x03, 0x9B, 0xBA, 0x58,
0x65, 0x57, 0x31, 0x28, 0x21, 0xB0, 0x07, 0x04, 0x02, 0xAE, 0x7C, 0x00, 0x00, 0x00, 0x00, 0x00 };
This does seem to include values for the addresses documented as "not used" - again, it's just a load of "Magic Numbers" with no explanation.
0x3D, 0x70, 0x23 gives 917 MHz
0x39 sets the datarate to 9.6 kbps
0x44 is the VCO register
0x03 is the modem register. UART mode is selected
0x9B set deviation to 4.95 kHz with shaping on.
The other registers are CC1070 specific and should not be anything you need to take into consideration when porting.